1116
1
Hello,
I’m trying to use a USB device with an STM32MP157C development board.
However, it didn’t work with the below msg.
(picture 1)

I found that error codes are printed when there is a kind of power problem.
After that, I boot the device connecting the serial port with my PC’s console.
I could find a Warning msgs like this.
usb 1-1: device descriptor read/64, error-32
I tried to replace the power source including the USB-C type, but the same msg printed
How do i solve this problem?
Thanks.
Best regards. Jo
Baozhu
2
Your picture doesn’t seem to show.You can provide more information about kernel dmesg, I can help you.
1116
3
Here is an error message.
(WARNING 500mA power supply detected Current too low, use a 3A power supply!)
Thanks.
Baozhu
4
I recommend using a debug serial port to connect it.This warning message simply prompts the user to use a better DC power supply.
1116
6
When I put my communication module to usb-A or C, it comes out with this message to serial port.
usb 1-1: device descriptor read/64, error-32
When I connect usb module to other linux devices, it recognizes as network interface and I can see it in ifconfig.
How can I fix it?
Thanks.
Best regards. Jo
Baozhu
7
Is there a DMESG log? Let me analyze it for you.