Hi,
I tested the odyssey x86 with a nvme disc, see below the results
[nls@nls-ody ~]$ iozone -e -I -a -s 100M -r 4k -r 16384k -i 0 -i 1 -i 2
Iozone: Performance Test of File I/O
Version $Revision: 3.489 $
Compiled for 64 bit mode.
Build: linux-AMD64
Contributors:William Norcott, Don Capps, Isom Crawford, Kirby Collins
Run began: Sun Jun 21 05:53:19 2020
Include fsync in write timing
O_DIRECT feature enabled
Auto Mode
File size set to 102400 kB
Record Size 4 kB
Record Size 16384 kB
Command line used: iozone -e -I -a -s 100M -r 4k -r 16384k -i 0 -i 1 -i 2
Output is in kBytes/sec
Time Resolution = 0.000001 seconds.
Processor cache size set to 1024 kBytes.
Processor cache line size set to 32 bytes.
File stride size set to 17 * record size.
random random bkwd record stride
kB reclen write rewrite read reread read write read rewrite read fwrite frewrite fread freread
102400 4 75576 98816 130944 131655 47150 95936
102400 16384 1297484 1292368 1553990 1537200 1610588 1257259
iozone test complete.
[nls@nls-ody ~]$