Does the case allow for the install of a 2.5" ssd? I have a spare sitting around I would like to use.
Yes, of course. 2.5" and 3.5" are fine.
Where does the case allow for this? There’s no place to put a 2.5in drive, let alone a 3.5 in one.
We will release the corresponding outer box and PCIE to SATA device.
So by that you meant they are not at all supported?
I purchased 3 of these cases because the listing said “the stackable structure allows you to stack more middle layers to create rooms very easily” which turns out to be completely false.
Do we have a time frame for the release of the corresponding outer box?