I ordered an OBD-II CAN Bus GPS Development Kit from Seeedstudio.
Firstly, it does not have the reset button as described on your web site.
Why does mine NOT have the reset button?
Secondly, I plugged mine in using a good USB-C connector and ran Putty on the port. Nothing comes up. My expectation is to see GPS data as described in your documentation.
Who do I NOT see any GPS data?
I cannot find any example code to enable the GPS and to log it. Please assist me in enabling the GPS and logging it to the SD card.
Please assist me in getting this device up and running.
Hi @cliftonkerr
The info@longan-labs.cc already answered your question.
Post the answer here so that other customers with the same problem can see it.
The description on our website doesn’t have the reset button, it is in the Longan’s website.
The reset button had been cancel in the latest version, but the Longan hasn’t updated the images on their website.
I plugged my unit into my computer using a good USB-C connector and ran Putty on the port. Nothing comes up. My expectation is to see GPS data as described in your documentation.
Why do I NOT see any GPS data?
3 Also, I was NOT able to find any example code that initialized the GPS. I was not able to find any code that prints the GPS or any code that saves the GPS.
Please assist me in getting the GPS and CAN working.
Longan: If you want to print the GPS, please try below code:
void setup()
{
pinMode(A2, OUTPUT);
digitalWrite(A2, HIGH); // power on
I tried the sample code and it still doesn’t work.
I had a much more detailed response, but this input box wouldn’t accept it; therefore, I’ve reduced the text.
The bottom line is that it still doesn’t work.
Hi @cliftonkerr
I’m sorry that you spent so much time searching so much information to obtain GPS data and Can data but did not get the results.
This product is from our supplier, and the guidance documents are also from the supplier.
I have reported the lack of detailed documentation to the supplier, and they will immediately modify the documentation to meet your needs.
Besides, the code I send to you before having something wrong, please check the below code.
void setup()
{
pinMode(A3, OUTPUT);
digitalWrite(A3, HIGH); // power on
The previous sample you gave used A2, which didn’t work.
Please explain what pinMode(A3, OUTPUT) is doing?
Is it turning on power to the GPS module?
This is extremely discouraging because it has taken me many many days to get this simple sample up and running.
Yesterday, I tried just enabling the CAN bus without GPS and the CAN data acquisition didn’t work. Do you have a simple sample to get the CAN bus working?
Hi @cliftonkerr
This means that the analog pin A3 is used as the output, and A3 is the corresponding correct pin.
The A3 pin controls a MOSFET to control the power of the system, including the power of the GPS. Pulling it high can make the MOSFET turn-on. If the GPS and other peripherals do not need to work, you can pull A3 low to save power.