NRF52840 Watchdog Reset code question

Hi there,
Are you using Arduino IDE?
either way if you call the Sleep function when the watchdog fires, the MCU will be reset.
Like this:

void goToPowerOff() {
  //sleepFlash();
  setLedRGB(false, false, false);
  Serial.println("Going to SLEEP System OFF  Tap to WAKE \n");
  display.clearDisplay();
  display.setCursor(10, 8);
  display.setTextSize(3);
  display.print("SLEEP");
  display.display();
  delay(500);
  display.clearDisplay();
  display.display();
  setupDoubleTapInterrupt();  // not needed here, if already applied..
  delay(2000);                // delay seems important to apply settings, before going to System OFF
  //Ensure interrupt pin from IMU is set to wake up device
  // nrf_gpio_cfg_sense_input(digitalPinToInterrupt(int2Pin), NRF_GPIO_PIN_PULLDOWN, NRF_GPIO_PIN_SENSE_HIGH);
  delay(2000);  // delay seems important to apply settings, before going to System OFF
  uint32_t pin = D2;
  pin = g_ADigitalPinMap[pin];
  nrf_gpio_cfg_sense_input(pin, NRF_GPIO_PIN_PULLDOWN, NRF_GPIO_PIN_SENSE_HIGH);
  delay(2000);  //15 seconds before turns off (if USB is plugged in, that circuit will still draw 2mA)
  Serial.println(" You're NOT doing anything, I'll Sleep.");
  delay(2000);
  sd_power_system_off();
  NRF_POWER->SYSTEMOFF = 1;
}

HTH
GL :slight_smile: PJ
be sure to change the HIGH NRF_GPIO_PIN_SENSE_HIGH to LOW and remove the delays that are noted for good Sleep!