Man, I am screwed. I got a Seeed Studio XIAO NRF52840 Sense, loaded CircuitPython on it. Then - because I’m stupid - I thought I’d re-format the board using the Windows format command. How much harm could THAT do?
Now:
- the board doesn’t show up on reset.
- When I double-tap the board’s RESET button to get to the Bootloader, I can see the board - XIAO-SENSE - and its default files.
- When I try to drag the micropython UF2 file into it, the load never completes and the board goes offline again
- If I try loading CircuitPython to it, no problem.
Anyone know a way I can turn back time?
Windows 11 Home (22H2), AMD Ryzen 9 7900X.