NRF52840 sense and bluetooth: tuya sensor refuses to show up?!

@zikken - With further investigation there are two possible issues I can think of…

  1. Scan responses are being filtered at the device (but would than mean NRF Connect would miss the advertisements as well?)
  2. The device is in basic operating mode (ie sleeps for 10s) then wakes and advertises.

Have a look here - this may be an option?