NRF52840 sense and bluetooth: tuya sensor refuses to show up?!

@zikken - I checked your code “as is” and it didn’t work.
Apart from the #include ArduinoBLE.h (probably a typo?) and the quotes around the peripheral.address() in the Serial.println, I find that the address filter should be set up first.

So…

void setup() {
  Serial.begin(115200);
  while (!Serial)
    ;

  // Init BLE
  BLE.begin();
  // Set up address filter
  BLE.scanForAddress(wanted, false);
}

void loop() {
  BLEDevice peripheral = BLE.available();
  if (peripheral) {
    Serial.println(peripheral.address());
  }
}

I don’t have the same (Tuya) device as you but if this doesn’t work I can create a BLE device here that uses “legacy” advertising.

Edit> I think the quotes around peripheral.address() may have been on purpose? If so, please ignore remark above :slight_smile:

Another Edit> I had an extra BLE.scan() which wasn’t required so removed it above.

1 Like