I’m trying to install a firewall, however it looks like nf_tables, ip_tables etc kernel modules are not included. I’m not familiar with working with the kernel, so it would be difficult for me to build my own kernel or whatever.
Does anyone know the easiest way to get a firewall running on this board?
I’ve never done it before and know very little about it, but after some searching it looks like I need to build a new kernel with these modules in place. And to do this I need the kernel source. Do you know if Seeed have released a guide for how they have built this image? They must do something kind of special, since fire-config is on the image. Looking around on it, it seems to be a modified image of BeagleBone Black Debian minimal image. But the size of the NPi image is a lot smaller, so there are definitely some things removed from it.
You mention the headers are available I can not find them anywhere. Can you point us to a wiki or download where this and/or other module recourse can be found?
I wasn’t able to figure it out either. I followed the digikey tutorial a couple of times, but that wasn’t working either.
It’s a good board, but the software / support around it is lacking. Search through the forums and everyone says the same thing.
I found another board from a company called Solidrun which is similar, only it’s more expensive. ClearFog Base. They provide multiple different images, as well as Armbian runs on it. So it’s a bit easier to get up and running with it.
It’s a bit disappointing because if it were not for the lack of kernel/module support it would be a good board. I also have tried the Digikey build process to no avail. I’ve also been struggling with replicating the image either SD or eMMC.
Definitely need to work on the support tools on this item.