Not booting after BIOS update on ODYSSEY X86J4105

Hi, I have left the board unplugged and without battery overnight. Plugged it back this morning. The power came on ( the blue light came on)… but nothing… for 30 minutes or more is not booting up at all.

I have others SBC (4 raspberry Pi running as NAS, PLEX server, VPN and Homeassistant) and never had issues when updating eeprom firmware.

I have seen in the forum that many users have problem with the BIOS update… The fans not working… not able to boot, issues with monitors… etc, etc.

I thinnk Seeed Studio is releasing updates without a proper test and quality control on the stability of what is being released.

This is my second odyssey… in the 1st one I was not able to connect the BT antenna and pins came bent… I returned it and bought a new one… It was working ok until I unfurtunately decided to update the BIOS following the published procedure. Now what I got is a Blue Box with a blue light… nothing else.

Really sad…