Nokia 7110 LCD Breakout Board

I am in the process of designing an Open Hardware breakout board for the Nokia 7110 LCD graphics display. These displays are available inexpensively on e-bay, and other e-stores.

I would like to fit this into the 5x5cm process, but it will be two small boards. One will be a simple clamping board, and the other will be the actual breakout board. Would it be possible to run this as a single 5x5cm Propaganda job if both boards fit into that area? I can leave the boards tabbed together, so that they can be processed as a single board, and broken apart later.