hi guys, *** hi seeed engineers ***
in addition to my last post (Arduin Uno + NFC Shield V2.0 = PN53x not found?!)
–> http://www.seeedstudio.com/forum/viewtopic.php?f=23&t=4898
i would like you to ask two things just to solve problems on my own,
and to be sure the shield is corrupted or (hopefully) not.
-
Which signals (Low, High) (or Analogue??) have to be send/given on which pins
of the shield to start(!) A SIMPLE reaction by the shield (just a *i am living)
without library, protocols etc…
I Explain: Similar to a sketch polling a pushbutton on Pin 12 and flashing LED on Pin13
on request! Or on which Pins someone can measure something (without danger)
when giving power to the shield (like a Power-on-self-Test in PC-BIOS) -
Which pins have to be wired to an host (arduino) to make the shield work
WITHOUT fixing it as a shield … for example with dupont-connectors???
Greetings & thanks in advance!