Nextion Basic NX4832T035 - Generic 3.5'' HMI 480*320 Touch Display for Arduino Raspberry Pi

Hi there,

So what’s the problem? of course it works Nothing special about those. Which BSP are you using? How did you connect it? Got a picture?
or Schematic?
If it works with a D1 , then YES it will work with ALL the Xiao’s I’m certain. It works Hardware Serial pass-thru to software Serial so where is the issue.?

HTH
GL :slight_smile: PJ :v:

I have it working in an old thread (air530) GPS module and a Xiao ESP32C3 & Nrf52840…:+1: