Nextion Basic NX4832T035 - Generic 3.5'' HMI 480*320 Touch Display for Arduino Raspberry Pi

Hi there,

So I was able to connect it up and happily even the touch screen works…

if anyone is interested I’ll put up the connection diagram, here are some pictures.
I didn’t test or setup the SSD but I’m sure it will work as well.


#include <SPI.h>
#include <ILI9486_SPI.h>
#include <Adafruit_GFX.h>
#include <bb_captouch.h>
#include <Wire.h>

// Touch Pins
#define TOUCH_SDA  22
#define TOUCH_SCL  23
#define TOUCH_INT  2
#define TOUCH_RST  17

// TFT Pins
#define TFT_CS     1
#define TFT_RST    0
#define TFT_DC     21
#define TFT_MOSI   18
#define TFT_SCK    19

// Some color definitions
#define ILI9488_BLACK     (0x0000)
#define ILI9488_WHITE     (0xFFFF)
#define ILI9488_RED       (0xF800)
#define ILI9488_GREEN     (0x07E0)
#define ILI9488_BLUE      (0x001F)
#define ILI9488_CYAN      (0x07FF)
#define ILI9488_MAGENTA   (0xF81F)
#define ILI9488_YELLOW    (0xFFE0)
#define ILI9488_ORANGE    (0xFC00)

// Screen dimensions (rotation = 3)
constexpr int SCREEN_WIDTH  = 480;
constexpr int SCREEN_HEIGHT = 320;

// "CLR" button location & size (bottom-right corner)
constexpr int CLR_BTN_WIDTH  = 80;
constexpr int CLR_BTN_HEIGHT = 40;
constexpr int CLR_BTN_X      = SCREEN_WIDTH  - CLR_BTN_WIDTH;   // 480 - 80 = 400
constexpr int CLR_BTN_Y      = SCREEN_HEIGHT - CLR_BTN_HEIGHT;  // 320 - 40 = 280

// "Home" button location & size (center of the screen)
constexpr int HOME_BTN_WIDTH  = 80;
constexpr int HOME_BTN_HEIGHT = 40;
constexpr int HOME_BTN_X      = (SCREEN_WIDTH  / 2) - (HOME_BTN_WIDTH  / 2);
constexpr int HOME_BTN_Y      = (SCREEN_HEIGHT / 2) - (HOME_BTN_HEIGHT / 2);

// Blinking "Touch Demo" variables
bool blinkState = true;
unsigned long lastBlinkTime = 0;
unsigned long blinkInterval = 500; // 500ms blink

// Track which "screen" or state we're in
// false = Initial screen (shows CLR only)
// true  = Cleared screen (draw allowed, shows Home button)
bool clearedState = false;

ILI9486_SPI tft(TFT_CS, TFT_DC, TFT_RST);
BBCapTouch bbct;

void setup() {
  Serial.begin(9600);
  while (!Serial);

  // Touch panel initialization
  pinMode(TOUCH_RST, OUTPUT);
  pinMode(TOUCH_INT, OUTPUT);
  digitalWrite(TOUCH_RST, LOW);
  digitalWrite(TOUCH_INT, LOW);
  delay(10);
  digitalWrite(TOUCH_INT, HIGH);
  delayMicroseconds(100);
  digitalWrite(TOUCH_RST, HIGH);
  delay(5);
  digitalWrite(TOUCH_INT, LOW);
  delay(50);

  bbct.setOrientation(270, 0, 480); // Top left
  bbct.init(TOUCH_SDA, TOUCH_SCL, TOUCH_RST, TOUCH_INT);

  // TFT init
  SPI.begin(TFT_SCK, -1, TFT_MOSI, TFT_CS);
  tft.setSpiKludge(false);
  tft.init();
  tft.fillScreen(ILI9488_BLACK);
  tft.setRotation(3);

  // Draw the initial screen
  drawInitialScreen();
}

void loop() {
  // Handle blinking of “Touch Demo” on both screens
  unsigned long now = millis();
  if (now - lastBlinkTime >= blinkInterval) {
    lastBlinkTime = now;
    blinkState = !blinkState;  
    drawBlinkingText(blinkState);
  }

  // Handle touch input
  TOUCHINFO ti;
  if (bbct.getSamples(&ti)) {
    for (int i = 0; i < ti.count; i++) {
      uint16_t tx = ti.x[i];
      uint16_t ty = ti.y[i];

      if (!clearedState) {
        // ====== Initial Screen Logic ======
        // User can only tap CLR
        if (isPointInRect(tx, ty, CLR_BTN_X, CLR_BTN_Y, CLR_BTN_WIDTH, CLR_BTN_HEIGHT)) {
          // Switch to cleared screen
          clearedState = true;
          enterClearedScreen();
        } else {
          // Do nothing if tapped outside CLR
          Serial.println("Tapped outside CLR button on initial screen - no action.");
        }
      } else {
        // ====== Cleared Screen Logic ======
        // 1) If tapped Home, restart
        if (isPointInRect(tx, ty, HOME_BTN_X, HOME_BTN_Y, HOME_BTN_WIDTH, HOME_BTN_HEIGHT)) {
          Serial.println("Home tapped, restarting...");
          delay(500); // optional
          ESP.restart();
        }
        // 2) Otherwise, allow drawing
        else {
          tft.fillCircle(tx, ty, 10, ILI9488_WHITE);
          Serial.printf("Touch => Drawing circle @ (%d, %d)\n", tx, ty);
        }
      }
    }
    Serial.println();
  }
}

// ----------------------------------------------------------------
// Screen / Drawing Logic
// ----------------------------------------------------------------

// Draw the initial screen with CLR button only
void drawInitialScreen() {
  tft.fillScreen(ILI9488_BLACK);

  // Title texts
  tft.setTextSize(6);
  tft.setCursor(0, 10);
  tft.setTextColor(ILI9488_GREEN);
  tft.println("Seeed Studio\n");

  tft.setTextSize(4);
  tft.setTextColor(ILI9488_RED);
  tft.println("4.0inch LCD");
  tft.setTextColor(ILI9488_YELLOW);
  tft.println("Res=480 x 320");
  tft.setTextColor(ILI9488_BLUE);
  tft.println("ILI9488\n");

  tft.setTextSize(4);
  tft.setTextColor(ILI9488_WHITE);
  tft.println("XIAO_ESP32C6");

  // Draw CLR button
  tft.fillRect(CLR_BTN_X, CLR_BTN_Y, CLR_BTN_WIDTH, CLR_BTN_HEIGHT, ILI9488_GREEN);
  tft.setTextSize(3);
  tft.setTextColor(ILI9488_BLACK);
  tft.setCursor(CLR_BTN_X + 10, CLR_BTN_Y + 5);
  tft.print("CLR");

  // Ensure blinkState is true initially
  blinkState = true;
  drawBlinkingText(blinkState);
}

// Switch to "Cleared" screen: only blinking text, plus "Home" in center
void enterClearedScreen() {
  // Fill screen black, keep blinking text
  tft.fillScreen(ILI9488_BLACK);
  // Re-draw blinking text according to blinkState
  drawBlinkingText(blinkState);

  // Draw "Home" button in center
  tft.fillRect(HOME_BTN_X, HOME_BTN_Y, HOME_BTN_WIDTH, HOME_BTN_HEIGHT, ILI9488_CYAN);
  tft.setTextSize(3);
  tft.setTextColor(ILI9488_BLACK);
  tft.setCursor(HOME_BTN_X + 10, HOME_BTN_Y + 5);
  tft.print("Home");
}

// Blink or erase “Touch Demo”
void drawBlinkingText(bool showText) {
  // “Touch Demo” near bottom
  int16_t xPos = 0;
  int16_t yPos = 280;

  tft.setTextSize(4);
  if (showText) {
    tft.setTextColor(ILI9488_WHITE);
  } else {
    tft.setTextColor(ILI9488_BLACK);
  }
  tft.setCursor(xPos, yPos);
  tft.print(" Touch Demo ");
}

// Check if (x, y) is inside a rectangle
bool isPointInRect(uint16_t x, uint16_t y, uint16_t rx, uint16_t ry,
                   uint16_t rw, uint16_t rh) {
  return (x >= rx && x < (rx + rw) && y >= ry && y < (ry + rh));
}

I 3D printed the Bezel from Glow in the dark PLA… Now you can find the console in the dark…:+1:

HTH
GL :slight_smile: PJ :v: