Hi everyone
I’ve just bought my first DS201 and after searching the internet I reckon this forum is my best hope for some good advice, so here goes.
My unit has a metal case, 8MB internal flash memory and the following specification:
Hardware version 1.0
MCU STM32F103VC
LCM ILI_9341
Firmware V3.28D
Here are my questions:
I understand from this forum that I can load rimidalv007 patched BenF 3.64 firmware and it will all work but won’t save files to the internal memory. Is that correct?
I’ve also read here that if I short pin 9 on the internal memory to ground then the firmware will think it’s an SD card and work properly. Has anyone tried this and does it work?
Thanx for asking (& answering!) these questions.
I’m a new Nano v3 owner myself, and this is the craziest “open source” piece of hardware I’ve ever seen (aside from a Chinese tablet PC I bought 2 years ago!!).
So I take it that your answer was that the firmware works, but grounding the pin didn’t, so you can’t save anything to memory? This info will help me decide if I want to replace my v3’s OEM 3.29 firmware and 4.22 software (app??).
It would also be nice if we had a list of what the firmware from 3.26 onward does/doesn’t do … anyone?