Newbie Qns about Seeeduino ADK Main Board

Hi all,

I’ve some questions about this board:

  1. Is Android (v2.3.4 and above) devices referring to Gingerbread & above? How can I check that my device is compatible?
  2. Connection from board to Android is via USB right? Can I use WiFi or Bluetooth instead?

Thanx.

A1. Yes, it works with Android v2.3.4 and above via Android Open Accessory API.
And it can work with Android OS 1.5 above wirh Android Debug Bridge
(ADB : developer.android.com/guide/deve … s/adb.html).

A2. Yes, Connect it from the USB-A port to Android device.
Yes, but you need Bluetooth/Wifi Module.

Thanks
Albert