New NPi i.MX6 crashes during Kernel init

Be that as it may, i’ve tried flashing with the SD image a couple of times now without succes and am still waiting for someone to say the image is actually functional… or even just give me checksum for it.

The image is called ‘imx6ull-debian-buster-console-armhf-latest-2gb’ but it is only about 350MB (extracted).

So after learning a lot and cursing even more:
U-Boot 2019.04-00676-gd447c486 (May 27 2020 - 05:26:26 +0000)

CPU: Freescale i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 49C
Reset cause: POR
Model: Freescale i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC… *** Warning - bad CRC, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:
Error: ethernet@020b4000 address not set.

Error: ethernet@020b4000 address not set.

Error: ethernet@02188000 address not set.
eth-1: ethernet@020b4000
Error: ethernet@02188000 address not set.
, eth-1: ethernet@02188000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
Checking for: /uEnv.txt …
Checking for: /boot.scr …
Checking for: /boot/boot.scr …
Checking for: /boot/uEnv.txt …
Card did not respond to voltage select!
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1…
switch to partitions #0, OK
mmc1(part 0) is current device
Checking for: /uEnv.txt …
Checking for: /boot.scr …
Checking for: /boot/boot.scr …
Checking for: /boot/uEnv.txt …
1587 bytes read in 9 ms (171.9 KiB/s)
Loaded environment from /boot/uEnv.txt
debug: [dtb=imx6ull-seeed-npi.dtb] …
Using: dtb=imx6ull-seeed-npi.dtb …
Checking if uname_r is set in /boot/uEnv.txt…
Running uname_boot …
loading /boot/vmlinuz-5.7.0-rc6-armv7-x5 …
10250152 bytes read in 456 ms (21.4 MiB/s)
debug: [enable_uboot_overlays=1] …
debug: [uboot_base_dtb=] …
loading /boot/dtbs/5.7.0-rc6-armv7-x5/imx6ull-seeed-npi.dtb …
38661 bytes read in 14 ms (2.6 MiB/s)
uboot_overlays: [fdt_buffer=0x60000] …
debug: [console=ttymxc0,115200n8 root=/dev/mmcblk1p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 vt.global_cursor_default=0 quiet] …
debug: [bootz 0x80800000 - 0x83000000] …
Kernel image @ 0x80800000 [ 0x000000 - 0x9c67a8 ]

Flattened Device Tree blob at 83000000

Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300c704
Modify /soc/aips-bus@2200000/epdc@228c000:status disabled
ft_system_setup for mx6

Starting kernel …

But it’s not going any further than this… Any idea where to start looking?