need the schematics of the respeaker core v2

can you provide the schematics of respeaker core v2 so that i can get a clear understand of how to configure the interface as my need?

Hi there,



We do not open source respeaker core v2 this moment. if you have any specific interface related questions, we can check it for you. thanks for understanding.



Bill

OK. I think it was CDC device though the only OTG device found is configured as a hub like the pasting below.

Is this the right port of the USB OTG interface?



T: Bus=01 Lev=00 Prnt=00 Port=00 Cnt=00 Dev#= 1 Spd=480 MxCh= 1

B: Alloc= 0/800 us ( 0%), #Int= 0, #Iso= 0

D: Ver= 2.00 Cls=09(hub ) Sub=00 Prot=01 MxPS=64 #Cfgs= 1

P: Vendor=1d6b ProdID=0002 Rev= 4.04

S: Manufacturer=Linux 4.4.138-respeaker-r0 dwc2_hsotg

S: Product=DWC OTG Controller

S: SerialNumber=30040000.usb

C:* #Ifs= 1 Cfg#= 1 Atr=e0 MxPwr= 0mA

I:* If#= 0 Alt= 0 #EPs= 1 Cls=09(hub ) Sub=00 Prot=00 Driver=hub

E: Ad=81(I) Atr=03(Int.) MxPS= 4 Ivl=256ms

Hi there,



Here is the schematic for the usb/pwr. thanks.







Bill

Hi! Can you publish all schematic at the current time? I was bought the board and trying to customize it, but it`s difficult w/o schematic…

Hi!Come from the ending of 2024, Can you publish the schematic now? I bought this board recently, and trying to customize it, but it’s difficult without the schematic

Hi there,
I don’t think it’s open source yet , SO you may need to reverse it DIY style…
:v:
GL :slight_smile: PJ :+1:

YET? what da? its been years… I think its just a standard Seeed one liner. Seeed products should be required to caryy a warning, sold as is, where is… what da?

A bit late to the party but I’d be interested to know whether Seeed ever plan on releasing the schematics to the ReSpeaker Core V2. I’d really like to know the pinout of the RK3229 Core Module as there appears to be absolutely no information about this module anywhere on the internet.