need master code for HW2.72

finaly I unbrick my dso203 but now the system ask the code each time power on the oscilloscope

need master code for HW2.72 and licence 9420c38f,

by unknown reason I can’t post and ask in minidso.com/forum.php?mod=fo … lay&fid=54
if anybody can give me the code, or ask code in forum I will be grateful

I have requested one there. Will update when they do.

thanks.

I can see your post in minidso.com forum : minidso.com/forum.php?mod=vi … a=page%3D1

repeat: many thanks

No problem.
Hopefully you will see reply soon. They are normally fairly responsive to these requests.

Yes, bobtidey. the reply was very soon too

and the code I need was B79102A1

now the devide works perfect

I am grateful. Thanks