Need help with RX/TX thread on HM-11 Android application

Since the HMCommAssist is not open source and I need to have directional communication with the Arduino and Android. I am willing to share the code if someone can help with the issue I am having. The issue I am having created a thread but now I can not transmit data to the arduino. Post a reply if you can help I will share the code via cloud.