Need help with Grove Serial Camera Code

To whom it may concern,

I recently bought a Grove Serial Camera and tried this
Grove_Serial_Camera_Kit
https://github.com/Seeed-Studio/Grove_Serial_Camera_Kit>/
SerialCameral_DemoCode_CJ_
OV528/.
I am using it with the Seeed Studio, Base Shield V2 103030000 Base Shield
V2, Arduino.
and a Wemos R1 D1.

I am not having any success and really need help, as this is an important
project for university. Could you please provide me some advice. It will be
highly appreciated.
Kind regards,
Frederik Cronjé

Tel.: +49 (0) 1701 13-6494
mailto:[email protected]

Hi

Frederik,


1. please take a picture about the hardware setup.

2. If you connect to hardware UART directly, you have to remove it when you download arduino program.


4. What kinds error message do you have?

Thanks

best rgds
Bill

Hi Bill,

Thank you so much, I managed to solve the problem. Now it is working
perfectly.
Kind regards,
Frederik Cronjé

Tel.: +49 (0) 1701 13-6494
mailto:[email protected]