Caster
March 20, 2022, 10:31am
1
I need advice on how to program RTC wakeup each day at specific time i.e. first the program should allow me to enter current date and time (e.g. 20.3.2022 13:25) and wakup time (hour e.g. 6:00) I need to wake up to update the display in the main loop and than go back to sleep.
I am inspired by dzonesasaki/xiao_sleepRtc.ino
Maybe I can use SAMD_TimerInterrupt too.
Caster
March 22, 2022, 7:38pm
2
It may help someone.
#include "RTC_SAMD21.h"
#include "DateTime.h"
RTC_SAMD21 rtc;
void setup()
{
rtc.begin();
Serial.begin(115200);
while (!Serial)
{
;
}
DateTime now = DateTime(F(__DATE__), F(__TIME__));
//!!! notice The year is limited to 2000-2099
Serial.println("adjust time!");
rtc.adjust(now);
now = rtc.now();
Serial.print(now.year(), DEC);
Serial.print('/');
Serial.print(now.month(), DEC);
Serial.print('/');
Serial.print(now.day(), DEC);
Serial.print(" ");
Serial.print(now.hour(), DEC);
Serial.print(':');
Serial.print(now.minute(), DEC);
Serial.print(':');
Serial.print(now.second(), DEC);
Serial.println();
DateTime alarm = DateTime(now.year(), now.month(), now.day(), 23, 0, 0);
rtc.setAlarm(alarm); // match after 0 seconds
rtc.enableAlarm(rtc.MATCH_SS); // match Every Minute
rtc.attachInterrupt(alarmMatch); // callback while alarm is match
}
void loop()
{
}
void alarmMatch()
{
Serial.println("Alarm Match!");
DateTime now = rtc.now();
Serial.print(now.year(), DEC);
Serial.print('/');
Serial.print(now.month(), DEC);
Serial.print('/');
Serial.print(now.day(), DEC);
Serial.print(" ");
Serial.print(now.hour(), DEC);
Serial.print(':');
Serial.print(now.minute(), DEC);
Serial.print(':');
Serial.print(now.second(), DEC);
Serial.println();
}
Caster
March 25, 2022, 9:15pm
3
This sketch works, the only problem is that the command myPowSave.begin(WAKE_RTC_ALARM); disables the GCLK module so the UART i.e. Serial.printf(“Fridge # %u”, tick); doesn’t work after wake up.
Any idea how to enable GCLK for UART to be able to use serial monitor after wakeup?
This code otherwise runs well:
// sleep and wake test using RTC
// for seeeduino xiao
#include "RTC_SAMD21.h" //install seeed_arduino_RTC : https://github.com/Seeed-Studio/Seeed_Arduino_RTC
#include "DateTime.h"
#include <EnergySaving.h>
EnergySaving myPowSave;
RTC_SAMD21 myRtc;
#define PIN_LED 13
volatile uint8_t tick = 0;
void setup()
{
myRtc.begin();
// Serial.begin(115200);
pinMode(PIN_LED,OUTPUT);
digitalWrite(PIN_LED,HIGH);//LED off (active LOW)
// myRtc.adjust(DateTime(2022, 3, 20, 19, 15, 0) );
myRtc.adjust(DateTime(F(__DATE__), F(__TIME__)));
myRtc.attachInterrupt(dummyfunc);
myPowSave.begin(WAKE_RTC_ALARM);
myRtc.disableAlarm();
DateTime timeNow = myRtc.now();
const uint16_t uiAlmNextSec = 10;
DateTime timeAlarm = DateTime(timeNow.year(), timeNow.month(), timeNow.day(), 6, 0, 0);
myRtc.setAlarm(timeAlarm);
myRtc.enableAlarm(myRtc.MATCH_SS);
}
void loop()
{
// for(uint16_t uilp=0; uilp<3; uilp++)
// {
// digitalWrite(PIN_LED,HIGH);
// delay(1000);
// digitalWrite(PIN_LED,LOW);
// delay(1000);
// }
// digitalWrite(PIN_LED,HIGH);
//bool run = UpdateDisplay;
//if(run)
//UpdateDisplay = !UpdateDisplay;
myPowSave.standby();
//proceed after wakeup
// Serial.printf("Hello World # %lu", packetnum++);
// Serial.begin(115200);
// Serial.printf("Fridge # %u", tick);
// Serial.end();
for(uint8_t uilp=0; uilp<tick; uilp++)
{
digitalWrite(PIN_LED,HIGH);
delay(1000);
digitalWrite(PIN_LED,LOW);
delay(1000);
}
digitalWrite(PIN_LED,HIGH);
// delay(3000);
}
void dummyfunc()
{++tick;}
Caster
March 27, 2022, 8:49am
4
Problem fixed. You must use Serial1.print instead of Serial.print The output will by at the pin 7 (TX) of the XIAO.