Hi all,
Im new to this forum and I have some confusing about the Msps. I want to buy a DSO Nano V1.6 from Ebay which says that the msps is 2.
cgi.benl.ebay.be/ws/eBayISAPI.dl … 0697737703
New advantages of hardware 1.6:
2) 1Msps -> 2Msps Sampling rate (Note: Supporting firmware is being developed
Max sample rate : 1Msps 12Bits (With the supporting firmware, max sample rate is 2Msps)
Is the BenF’s firmware written to handle this 2Msps or is the ebay site just telling crap?
Kind regards
I have checked the datasheet , it is 1M