My XIAO ESP32S3 with camera attached is overheating

Hi,

I’ve just received my XIAO ESP32S3 Sense from Mouser. When I first uploaded the camera streaming example from the Seeed wiki, I noticed that the ESP32S3 board heats up very quickly. I implemented the reading of the internal temperature sensor with an external temperature probe attached to the bottom of the board. I found that the ESP32 is overheating rapidly, with the internal temperature exceeding 80°C and the external temperature reaching over 95°C+ before I disconnected it. With the camera board disconnected, the measured internal temperature was around 60°C and external was about 55°C. With the camera board but without the attached camera, the temperature reached 67°C. With the camera itself attached to the camera board but not initialized, the temperature hit 75°C in a short time. When I initialized the camera with streaming, the temperatures skyrocketed past 80°C, as I described earlier.

Sorry, but I believe the XIAO ESP32S3 Sense board design is flawed. I don’t really know which specific IC generates so much heat, but I suspect the voltage regulator, based on the rising temperature even without the camera attached. It’s undeniable that the ESP32 generates a lot of heat, but this amount of heat is concerning. Without schematics, I can’t pinpoint the problem. With such a tight hardware layout and grounding, it’s impossible to discern which IC contributes to heating up the board. All I can say is that I can’t run camera streaming indefinitely, even with a copper heatsink.

I really hoped that the board would be cool with all the work you’ve done to design it, but I can’t use it. It will destroy itself without any modifications or a huge cooling solution.

Best Regards,

Electry

I THINK IT GETS HOT WE HAVE SEEN THIS WITH THE camera working it is a very processor intensive

Yeah, but why it is so hot even without initialized camera?

The ESP32 was idling while board goes to 75°C and rising.

Just the difference between “the idle ESP32 board without cam/SD addon” and “the idle ESP32 with cam/SD addon and ov2640 attached” is 20°C+. In both mentioned scenarios, the Wifi AP and printing of the internal temperature into the USB serial port every 1 second were active.

The heat has got to be coming from processor power, its not like an internal short circuit or something so the problem is in the code, its trying to do too much, so i dont think it is hardware specific

You can also choose this camera with heatsink to mount on xiao esp32s3 sense

Anyone tested this board for face recognition?

Hi,

I just got my hands on another board supporting a camera out of the box, and the temperature was acceptable (under 50 °C) even after hours of camera streaming. It uses ESP32-S3 on the module instead of the chip directly on the board, but this info only points out there might be a flaw in the hardware design of the XIAO with ESP32-S3.

This post is not an advertisement, just an example of how cold an ESP32-S3 with a camera can run. I just added a periodic printout of internal temperature to the unused main task loop (in the camera stream example) with a period of 10 seconds. I measured the external temperature too and it was about 6 °C lower. https://1drv.ms/i/s!Ai_4aucnnOOOj8lSNrHBmKb-CROZjA

Best regards,
Electry

I have tinker ai cam. I am not able to use face detection and recognition

Yeah, I can confirm. A face detection feature in the example always crash on any of my ESP32 boards with camera. IDK why, I didn’t try to debug it.

Sadly, I am convinced that a different camera can’t change the XIAO ESP32-S3 Sense board is overheating. I used different cameras of the OV2640 type. The XIAO ESP32-S3 Sense always overheats and is hot even without it. The camera works as expected and gets only slightly warm duting prolonged use. So there is no point in a purchase of another camera type. I am more interested in global shutter cameras. I work with fast robots like small autonomous racing cars and drones.

Electry

I started playing with Xiao ESP32-S3 sense. I see same poor thermal performance. Even with 1x1x0.5cm heatsink from stepper motor driver the temps are quite high. Just streaming i2s audio and not having sense board attached causes temps to be around 55C. Adding sense board and limiting fps for camera image to 1fps makes temp hover around 60-62 (800-600 res). Doing anything above 1fps makes temps skyrocket well above 65 which is the rated temp for this xiao module. For me the camera on this board is not usable for this reason.
I will still use the board a bit more to see what can be done with it but this thermal issue is a dissapointment for me. This may be due to compactness and power delivery chips (xiao has some buck converter which may run hot and sense board have two LDOs which need to burn some of the voltage into heat). The board mentioned by @electry has some dedicated PMIC doing all the power delivery so it may be better thermalwise.
If anyone has those issues and knows of some smart solution (other than slapping and intel cpu cooler on this) I am all ears.

I think this thermal issue is confirmed. I bought 2 Xiao ESP32S3 board and both of it getting overheat just running some simple BLE scan. I thought I did somethin wrong and check my wiring again and again. Is there any clarification from seedstudio?

the code needs to be optomized do some load testing

Heat problem might be solved using heatsink. But I didn’t expect this to be implemented on microcontroller scale. Another aspect is, I need it for low power application using battery and solar panel. With this amount of heat generated, I doubt it will suit for application that need low power. Code is basically still example from arduino sketch with minimum modification.

yes you will have to cut the bloat out of the code… high power applications will not be compatable with low power applications

Hi there,
I’m gonna hook up the power profiler to it, We need someone with a thermal camera to scan the thing with the demo web cam server running. the one I have get HOT!(as in you can’t touch it after a few minutes)
I’m sure it would melt any PLA 3D printed enclosure. I swear this was just an attempt to answer the ESP-CAM and it’s more of a gimmick than serious usable tech. Great for a demo only. IMO.

we’ll see
GL :slight_smile: PJ :v:

YES I agree… but my point is the code was recycled as well and is bloated… Seeed is well known for hardware but also well known for software (winkwink) Just the upload of the blink sketch takes hours

there is nothing wrong with the hardware, like direct short or heating resistors… the heat is coming from the processor… like an old dell laptop which will catch fire while trying to upload the contents of your personal data to the cloud for no apparent reason.

my suspecion is the dual core setup where half the device is managing the Coms and the code is bloated resulting in excessive and basicly unnecessary process allocation… maybe even some type or ram sink… almost like how ram sink can burn up a HDD because the processor keeps asking for more ram and the disk keeps paging worthless ram out… i understand the device does not have ram or hard drives… but that is solid state analogy… I dont know enough about the programming to take it any further…

I’ve tried several ESP32 type camera boards and they all get extremely hot. But then ran across and AMB82 Mini. No, it’s not ESP32x based. But blows all of them out of the water. Especially if you see the YouTube comparison. It runs cool and does a lot more.

That said, I wondered about changing the processor speed on the ESP32x versions might help cool it down.

The main power use, and thus heat generator, are the camera themselves, they do use a lot of current when they are active. The ESP32S3 processor itself only uses circa 35mA when running and thats no really going to make it ‘hot’.

If you change the camera to an OV3660 you can put the ESP32S3 into light sleep and camera into standby and it uses circa 3.5mA.

Did anyone try to power the module directly with 3.3V (from a buck converter that is able to provide enough current) instead of 5V from USB?

I would expect, that the ESP32S3 attached with camera module can run significantly cooler because the onboard LDO converter from 5V → 3.3V no longer needs to convert voltage difference into heat.