MW0582TR11 Not Working...

Yes, I have downloaded the latest SDK from Git. The problem I’m having right now is that there isn’t any data being sent by the unit when it is powered up. I get the screen of default settings but the unit will not send any data. The SDK app doesn’t contain any commands that start the sending of data. There are commands to change the settings, but that is it. So I’m ASSUMING that the unit will automatically start sending data since there aren’t any commands to do so. I would like to get a full list of commands that this unit responds too beyond that what is listed in the Read.me file or the app.