Music Shield with Etherten Freetronics board

Hi all ,

I have a SeeedStudio Music Shield which im trying to use with a freetronics Etherten controller board, the problem im having is that the music shield is erroring out on boot with SD card init failed. I also have a arduino Uno which it is working on but i would really like to use the etherten as i plan on using the Network side of it. Does any one have any sugestions on how i could get it to work on the Etherten?

Thanks in advance.
Mack

Didn’t play with Etherten board, but there may be some conflict while operating the SD card the Ethernet Chip, as they both use SPI interface.