Music shield v2

Hello
I’m interested in whether can I play music from a given time with music shield 2 and arduino. And if I can, how, just tell me function from the library which takes time argument to start playing from that time.

It includes many features:
1 some play modes: MODE_NORMAL、 MODE_SHUFFLE、 MODE_REPEAT_LIST、 MODE_REPEAT_ONE , play selected song

2 Basic functions via button or software: play, pause, stop, next song, previous song, volume adjustment, FastForward, FastRewind

And more information you can visit the wiki of Music Shield v2: seeedstudio.com/wiki/Music_Shield_V2.0

Jacket