E3po
June 16, 2011, 12:15am
1
hello! I am curious to see if anyone has had the shield powered by the dock connector?
I have a bose dock and I can play music but still need external power. Also curious if the unit could possibly recognize the dock’s remote for advance tracks.
Thanks!
-e
Yes, it can. But it can be remotely controlled only when it work with ATmega328 based Arduino board.
You can follow the instructions here:http://garden.seeedstudio.com/index.php?title=Music_Shield#Software_Installation
E3po
June 22, 2011, 3:11am
3
Thanks Steve!
I have the music shield working.
It does not get power from my dock, but my ipod does. Any suggestions as far as modifying code?
Thanks
-e
E3po
June 23, 2011, 1:07am
4
The software has a line that says:
mySerial.begin(19200);// used for receiving command data from the iPod dock.
does that include power?
If you know a dock (make and model) that does in fact power the unit and the arduino please let me know.
As I said before, the dock I own powers my ipod but not the music shield or arduino.
I could not even get the shield to function properly on ANY arduino other than MEGA 1280. (I tried MEGA 2560, UNO, and Duemilanove also)
Please help.
-e