Music Shield pins D0-D9 - How to use for my own application?

When I copy and commend the code for InitIOForKeys() to InitIOForKeysCustom() like below, music plays briefly as the volume turns all the way down. As if the volume down button was pressed.

[code]// This library is free software; you can redistribute it and/or
// modify it under the terms of the GNU Lesser General Public
// License as published by the Free Software Foundation; either
// version 2.1 of the License, or (at your option) any later version.
//
// This library is distributed in the hope that it will be useful,
// but WITHOUT ANY WARRANTY; without even the implied warranty of
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
// Lesser General Public License for more details.
//
// You should have received a copy of the GNU Lesser General Public
// License along with this library; if not, write to the Free Software
// Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA
#include <avr/io.h>
#include “config.h”
#include “filesys.h”
#include “player.h”
#include “vs10xx.h”
#include “record.h”
#include <SoftwareSerial.h>

SoftwareSerial mySerial(2, 3);//pin2-Rx,pin3-Tx(note: pin3 is actually later used as volume down input)

//Initialize IO control ports of KEYS
void InitIOForKeysCustom()
{
// DDRD &= ~(1<<VD);
DDRD &= ~(1<<BK);
DDRD &= ~(1<<PS);
DDRD &= ~(1<<VU);
DDRD &= ~(1<<NT);
//internal pull-high
PORTD |= (
// 1<<VD |
1<<BK | 1<<PS | 1<<VU | 1<<NT);
}

void setup()
{
Serial.begin(9600);
//Serial.println(“Hello test!”);
mySerial.begin(19200);// used for receiving command data from the iPod dock.

InitSPI();

InitIOForVs10xx();

InitIOForKeysCustom();

//InitIOForLEDs();

InitFileSystem();

//VsSineTest();

Mp3Reset();

}

void loop()
{
#if defined(AVR_ATmega1280)|| defined(AVR_ATmega2560)
// If play/stop button is pressed during boot, enter recording.
if (0== PSKey)
{
delay(20);
while(0 == PSKey);
delay(20);
Record();
}
#endif

Play();
while(1);
}

[/code]