Music Shield not playing

Hi,



I followed the post exactly and deleted the libraries required and the unziped the new libraries into the correct location. I started again with a fresh Arduino 1.0.2 install and these are the only two libraries I have added. I now get a compile error like below.



In file included from MusicPlayWithName.ino:39:

C:\Users\jeremy.PSY\Dropbox\arduino-1.0.2\libraries\MusicShieldNewSDLib/newSDLib.h:28: error: ‘SdCard’ does not name a type

C:\Users\jeremy.PSY\Dropbox\arduino-1.0.2\libraries\MusicShieldNewSDLib/newSDLib.h:29: error: ‘Fat16’ does not name a type