Hello,
I have tried various MusicPlayer libraries from Seedstudio and I am still unable to compile any of the examples.
The one which left me with the least error is apparently v1.0 but I am unable to resolve the remaining error below:
Arduino : 1.6.7 (Windows 7), Carte : “Arduino/Genuino Mega or Mega 2560, ATmega2560 (Mega 2560)”
In file included from C:\Users\JP\Documents\Arduino\libraries\MusicPlayer\examples\creatList\creatList.ino:33:0:
C:\Users\JP\Documents\Arduino\libraries\MusicPlayer/MusicPlayer.h:66:26: error: ‘playingstatetype playingState’, declared using anonymous type, is used but never defined [-fpermissive]
extern playingstatetype playingState;
                      ^
C:\Users\JP\Documents\Arduino\libraries\MusicPlayer/MusicPlayer.h:65:3: error: ‘typedef volatile enum playingstatetype’ does not refer to the unqualified type, so it is not used for linkage [-fpermissive]
} playingstatetype;
^
Plusieurs bibliothèque trouvées pour “Fat16.h”
Utilisé : C:\Users\JP\Documents\Arduino\libraries\Fat16
Non utilisé : C:\Program Files (x86)\Arduino\libraries\Robot_Control
exit status 1
Erreur lors de la compilation.
Ce rapport contiendrait plus d’informations si l’option
“Montrer les informations de sortie pendant la compilation”
était activée dans Fichier > Préférences.
Can someone help me?