Just for the sake of keeping my progress up to date
I will really only be working on this during weekends. Attached is a sketch and the required libraries to just get the music shield working. It is poorly coded but works reliably. It doesn’t even have controls
but is compatible with SD, SDHC and SDXC (up to 2TB) and works with the Mega.
EDIT: I said poorly coded, it may be ONLY Mega compatible. UPDATE: Since the SD library handles SPI, it should be fully compatible with all arduinos using the default music shield pin out.
My goal is to create a library that is:
- Simple
- Compatible with all Arduinos
- SD, SDHC and SDXC Compatible - Complete
MusicLibrary.zip (128 KB)