Music Shield - Card Find Error

hey boy

  1. Please notice the red words:The library of Method 1 is not the same as the library of Method 2.When you use Method 1, make sure that there is no the library of Method 2 in… Arduino-1.0\ libraries. In other words, when you use one of the methods, ensure you have removed the library files of another method.Delete and coverage is not the same, so make sure your operation is deleting instead of overwriting.

The libraries of Method 1 is totally different from libraries 2.

2)Maybe you SD Card can’t fit our Music Shield.

3)Usernames? our forum? i’m sorry you may not change your usernames.

Any problem ,please let’s know. :slight_smile: