thanks deray
It sounds to me I can put Ethernet shield on the MEGA, then MUSIC shield on the Ether shield. Is it?
Is it fine for not connecting ISP (6pin::MISO\SCK\RST\VCC\HOSI\GND) to Music Shield??
Thanks again!
If both Music Shield and Wiznet Ethernet shield need ISP interface for talking to MEGA,
When I joint these two shield together, will it cause conflicts???
yeah,you can joint these two shield together. but you must change the on of the D10 (Used for SPI Chip Select.pin) , because both of them use the same chip select.ping.