Hello, we have an application where we need to add 2x M.2 cards inside,
It´s a m.2 Card that supports 4xCAN controllers, and we need to have 8xCAN into the system to create a standalone 8xCAN bus data logger.
CAN interface for the M.2 slot (uses PCIe lane)
4xHigh-speed CAN channels (ISO 11898-2)
Form factor M.2 type: 2280/2260-B-M
It seems that the Card is using one PCI lane when we look to the API´s.
Do you know if there does exist any card to extend the number of M.2 slots?
Thanks for your help!