Dear Friends,
I’m starting with the development for the MT3620 MCU. Among other things, I have an Grove - 4 Digit Display to test. But I’m a little bit confused.
I I’m following the tutorial at http://wiki.seeedstudio.com/Grove-4-Digit_Display/. I downloaded the Grove 4 Digit display library from here: <LINK_TEXT text=“https://github.com/Seeed-Studio/Grove_4 … master.zip”>https://github.com/Seeed-Studio/Grove_4Digital_Display/archive/master.zip</LINK_TEXT>
After adding the library to my project in Visual Studio, I can include the TM1637.h header file. But when trying to build the solution, the following error happens:
Severity	Code	Description	Project	File	Line	Suppression State
Error	MSB6006	“arm-poky-linux-musleabi-gcc.exe” exited with code 1.	Mt3620Blink1	C:\Program Files (x86)\Microsoft Visual Studio\2017\Community\Common7\IDE\VC\VCTargets\Application Type\Linux\1.0\AzureSphere.targets	91	
Besides of that, I looked into the TM1637.h and .c files, and I found includes like #include <Arduino.h>. THen my question is, is this the right library to use the 4Digit display with an MT3620? Maybe this library is suitable only for Arduino.
Or I am missing something? I have to admit that I’m a newbie in C development.
Thank you in advance
Hi Friends,
Please check <LINK_TEXT text=“http://wiki.seeedstudio.com/Azure_Spher … phere-demo”>http://wiki.seeedstudio.com/Azure_Sphere_MT3620_Development_Kit/#azure-sphere-demo</LINK_TEXT>. thanks.