Thanks for the tips.
I have not had the LED on. It’s kinda neat to play with, but I am not convinced that there is a lot of practical value in that feature.
- I have replaced the power supply with a (hopefully) clean power block and will test some more.
- It’s hard to change the ambient temp, and in any case, I need it to work at least up to ~25C…
- I will check the orientation if the power doesn’t help.
Do you know what the Height Threshold and Sensitivity control exactly? I have looked in the code, and the Sensitivity numbers are translated to larger numbers, e.g. {1, 2, 3} = {3, 15, 30}, but not sure exactly what these represent… number or readings/frames to average over? Higher number is more sensitive?
FYI, the other unit is a C1001 from DFRobot. I built a custom component for HA for it, but it seems to be quite unreliable. Maybe as I gain more experience with this unit, that one will make more sense…
Thanks again.