MR60FDA2 can't be flashed anymore

[quote=“umaiku1, post:1, topic:292028”]

Hi, there must be some general problem.
I use MR60BHA2 and updated by the correct latest firmware (MR60BHA2_eeprom_1.6.12.bin) from the web page seeedstudio and after finished update my module stuck in the exact same state. I cant work with radar and it is stuck in the bootloader. Therefore I think there is not only problem with different firmwares.
Currently I see the big difference between old 1.6.10.bin size 43084 byte and 1.6.12 size 32192 byte. This seems to me some problem with file, but uploader must check integrity of the file before poceed upload.

Martin