MR60FDA2 can't be flashed anymore

I bought the MR60FDA2 and tested it. Results for Fall Detection was not great. Then I saw that an update exists, so I updated it, but results were not much better.
I then realized that the MR60BHA2 was the same hardware and so I tried to flash the firmware and since then, I can’t do anything anymore, it seems like it keeps sending the same information, but I can’t flash it anymore. What can I do now to restore it, or is it bricked??

Hi there,

And Welcome here…,

SO more than likely it is Bricked if you wrote Firmware not Partitioned for the correct device, they are NOT the Same one is an early release. Heartbeat , Fall and Breathm, the other is just Fall and presence detection.
If you wrote just the Xiao firmware , sure you can un-brick it, If you change the Radar firmware , I don’t think it can be. So I would enter Bootloader Mode and see if anything is alive . If so reflash with the Proper firmware and test it again, Are you using the correct Baud Rate? the Default is 115200 ?

HTH
GL :slight_smile: PJ :v:

Hi and thanks for your quick response.

The Xiao works well and is programmed with the passthrough mode program. But I can reprogram it with any other program, that’s not a problem.
I programmed the radar firmware first with MR60FDA2_eeprom_v4.0.18.bin and then with MR60BHA2_eeprom_1.6.4.bin. Now it keeps sending on the OTA upgrade tool the information on my screenshot but doesn’t go in to update mode to receive a new firmware.
And yes, I used 115200 Baud Rate, but I also tried changing it to see if something happens, but there is nothing happening…

1 Like

Hi there,

Yes, I was afraid of that… No method exist AFAIK, maybe Seeed can Comment. There may be some Power UP , force Flash LOAD process with Radar only that is possible. However it may require connection to the bottom pads for SWI.?

HTH
GL :slight_smile: PJ :v:

Yes, as PJ_Glasso mentioned. Although the hardware is the same, the software is completely different. Using different firmware across devices is not allowed, as it may cause damage to the radar.

OK, so what do I do now? The hardware is not damaged, it sends regularly information (as seen in my screenshot above), but I can’t “Request Update” anymore.
How can I reprogram it now? I really hope it is possible, otherwise I find it crazy that such expensive hardware not only doesn’t work properly but also can’t be reprogrammed…

I also “asked around” and ChatGPT gave me almost exactly the same answer.
Unfortunately, it is completely useless because:

  1. The MR60FDA2 only has a Reset button
  2. The MR60FDA2 has a USB-C port which can only be used for powering, not programming the EEPROM
  3. There is no “Force Upgrade” or “recovery mode” buttons on the tool
  4. The MR60FDA2 is used (and programmed) using an XIAO- ESP32-C6, and there should be a way to program the EEPROM through RX/TX or I2C using the XIAO.

So by writing in to this forum, I was hoping to get the last part of ChatGPT’s answer, that is: They may provide a special recovery image or guide you to a deeper UART recovery process.

So is there anyone from Seeed that can help here, or do I need to contact the support outside of this forum?

I would really appreciate if someone from Seeed could give me an answer!

1 Like

Hi there,

So your reply sounded a TAD salty :rage:, for trying to help…
I’ll ask plainly did you even understand any of it ? did you try it, any of it. ? You don’t want to answer that’s fine too, but YOU are the one who wrote the wrong file to it, so if you know something more how these devices work as I do, be glad I replied at all. :face_with_hand_over_mouth:

GL :slight_smile: PJ :v:

for example, Hold the reset button and plug in usb ?
I bet you didn’t…because you would have said so. :lying_face:
Also now after looking at the schematic , I would wager IT CAN be restored using an external Probe easily. The pins are there the bin file is also and Now I see in the pic, They are on the bottom. :+1:

The more I look at it, hell you may not even need the probe…:grin:
That is to say… You only bricked or looped the OTA.

I have tried pulling BOOT1 to ground and to VCC while powering the XIAO and nothing happens.
I don’t have a USB-to-Serial adapter, but as the XIAO is anyways connected to it, it could flash it, if I had the right program to do it.

I’m going to contact Seeed support directly, as this is going nowhere here.

1 Like

Hi there,

LOL, WHy "Boot1 to GND, it’s already pulled low.
did you read a schematic?
GL :slight_smile: PJ :v:

I did the same thing as @umaiku1, but I believe I did it in the opposite direction (flashed MR60FDA2 on MR60BHA2 hardware.) I am seeing the same behavior in Seeed OTA as @umaiku1 .

I was wondering, did you get a response from seeed? did they help you unbrick?

If the bootloader is intact (which it seems to be), you can likely re-flash it using the correct firmware for MR60FDA2.

Switch to OTA Mode in the flashing tool (you already have it selected).
Ensure baud rate is correct – try 115200 if 9600 doesn’t respond.
Click “Request Update” to initiate the OTA handshake.
If it responds and enters OTA update state, select the original firmware (specific to MR60FDA2) via “Open File” and flash it.
If OTA fails, try UART mode instead.

We have updated the recovery method, please refer to:
https://files.seeedstudio.com/wiki/mmwave-for-xiao/mr60/Radar_Firmware_Recovery_Method-Jlink.zip

And, we have clearly labelled the risks on the documentation in the hope of reminding people not to use the wrong firmware illegally. Even if there is a way to recover it, the price to pay is extremely high (e.g. you need to buy a JLINK)

1 Like

For anyone planning to update firmware on the MR60FDA2 or MR60BHA2:
I’ve reverse-engineered the MR60BHA2 and the underlying HiLink radar. Seeed Studio’s manuals were very helpful.

In any case, I can confirm that you should not flash an MR60FDA2 with the MR60BHA2 firmware, and vice versa. The hardware differs (the ADT6101P chip is configured differently).

I also wrote a cross-platform Python utility that simplifies firmware updates:

[github_com]/SergeyZh/hlk-ld6002-adt6101p-internals/blob/main/docs/firmware-update.md

3 Likes