I followed instructions according to seeed wiki page:
https://wiki.seeedstudio.com/ha_with_mr60bha2/
I was able to connect 2x mmWave sensor with XIAo ESP32-C6 into HA but some entitites are not showing? only illuminance and the light switch work.
I’m missing hear rate, respiratory rate, person information entitites?
Check if you’re using the correct ESPHome YAML provided in the wiki or updated from the official Seeed GitHub repo:
You should have flashed a YAML like:
uart:
rx_pin: GPIOX
tx_pin: GPIOY
baud_rate: 115200
sensor:
- platform: custom
lambda: |-
auto my_sensor = new MR60BHA2();
App.register_component(my_sensor);
return {my_sensor->heart_rate_sensor, my_sensor->respiratory_rate_sensor};
sensors:
- name: "Heart Rate"
- name: "Respiratory Rate"
I used the firmware from the wiki pages and followed the instructions from there. This procedure provided no YAML, I guess all is setup on the hardware?
I tried via ESPHome builder but got stuck as well, would you have a complete YAML example to share?
I used the MR60BHA2 Yaml example from the Wiki and I had to remove the LED from the Yaml or I receive
INFO ESPHome 2025.5.1
INFO Reading configuration /config/esphome/res01-hr-rr.yaml…
INFO Updating https Failed config
light.esp32_rmt_led_strip: [source /config/esphome/res01-hr-rr.yaml:67]
platform: esp32_rmt_led_strip
id: led_ring
name: Seeed MR60BHA2 RGB Light
pin: GPIO1
num_leds: 1
This feature is not available for the IDF framework version 5.
rmt_channel: 0
rgb_order: GRB
chipset: ws2812