MR60BHA2: failing to get arduino examples to work

I bought a MR60BHA2 and I am able to get it into Home Assistant via ESPHome (it arrived flashed in this way). I want to develop my own sampling / publishing solution and thought to go via Arduino, following the examples and adapting them.
I can compile and upload the code, no issue, but then I see nothing on the Serial monitor and I cannot even run the blink example. I tried several solutions and eventually thought that maybe the issue is the Serial, but everything works (I tried the WiFi example but nothing connects to the WiFi …) … but no.

I am sure I am making a stupid mistake somewhere, but I am not finding a way out of the corner. I succeded in re-flashing back the provided seeed-studio firmware to get the thing work with HA and ESPHome, but this is not what I want … I am making my own platform and I need to be able to program access to WIFI and MQTT …
Is anyone able to help? Thanks in advance.

What code are you using? After uploading the program, did you reset to ensure it runs?

Thank you for checking :slight_smile:
I succeeded yesterday in getting the sensor to run the code compiled and uploaded with arduino. To be honest, after the n-th trial I do not know how I got the device to work, but at least it does. Thanks

It must match Serial.begin(baudRate) in your sketch (default for ESPHome is usually 115200, but some examples use 9600).
Ensure Serial Monitor is Closed During Upload.
Try a minimal working sketch:

void setup() {
  Serial.begin(115200);
  delay(1000); // Wait a bit for Serial to initialize
  Serial.println("Booting...");
  pinMode(LED_BUILTIN, OUTPUT);
}

void loop() {
  Serial.println("Blink");
  digitalWrite(LED_BUILTIN, HIGH);
  delay(500);
  digitalWrite(LED_BUILTIN, LOW);
  delay(500);
}

Open Serial Monitor at 115200 baud and look for output. The problem may happen due to wrong SSID/password. It is also possible that WiFi.begin() is not being followed by WiFi.waitForConnectResult() or while (!WiFi.isConnected()) {...}

If you want to keep all info about MQTT always handy, you can see here: ESP32 MQTT - The Engineering Projects