We always face with some applications which needs to just send some data to a server. To start thinking about MQTT-based framework, here’s the application scenarios:

What’s MQTT
MQTT is a machine-to-machine (M2M)/”Internet of Things” connectivity protocol. It was designed as an extremely lightweight publish/subscribe messaging transport. It is useful for connections with remote locations where a small code footprint is required and/or network bandwidth is at a premium. For example, it has been used in sensors communicating to a broker via satellite link, over occasional dial-up connections with healthcare providers, and in a range of home automation and small device scenarios.
Pub/Sub Model

Figure: Pub/Sub pattern
In a pub/sub model, the producer acts as publisher, and consumer acts as subscriber. Using the publish – subscribe pattern in application can dramatically simplify its design and improve testability.
In a distribute IoT system, basically you just have some part(s) of your device subscribe to a particular topic and have some other part(s) of your device publish messages with that topic. Messages sent will be delivered to all registered handlders (aka listeners, also receivers) for a given topic(one-to-many broadcast).
We implement the following parts:
1.Node
MeshBee is a low-cost, community-supported, programable zigbee wireless development platform, aim at mesh network applications. It’s simple enough to send a heartbeat to the Coordinator installed on Gateway. Visit here to get some programming guide.
1.1 Generate a heartbeat in AUPS
every node can produce something, adc value, temperature etc.
Edit ups_arduino_sketch.c:
[code]ANALOG_T adc_pin;
void arduino_setup(void)
{
//Init your device here
}
void arduino_loop(void)
{
uint8 tmp[sizeof(tsApiSpec)]={0};
tsApiSpec apiSpec;
int16 temper = vHAL_AdcSampleRead(E_AHI_ADC_SRC_ADC_3);
sprintf(tmp, "gas:%ld\n", temper);
PCK_vApiSpecDataFrame(&apiSpec, 0xec, 0x00, tmp, strlen(tmp));
/* Air to Coordinator according to mac address */
uint16 size = i32CopyApiSpec(&apiSpec, tmp);
if(API_bSendToMacDev(0x00158d000035529c, 1, 1, tmp, size)){
suli_uart_printf(NULL, NULL, "<HeartBeat%d>\n", random());
}
}[/code]
In example above, we sample pin AD3 periodically, and call “bSendToMacDev” to send the value to the Coordinator(mac address of coordinator is ’0x00158d000035529c’).
The heartbeat format gateway requires is key-value pair string (KVP).
“key:value” + ‘\n’
eg: “temperature:23 \n”
Heartbeat is sent with no ack.

Figure: Network Topology
1.2 Active MCU mode
When we finished the heartbeat generator module in AUPS, we must activate the MCU mode to send heartbeat.
Type “+++” at AT console.
Setting interval of AUPS thread by “ATMF xx”
Enter MCU mode by “ATMC”
2.Gateway

Figure: Gateway software architecture
Gateway is written by pure Python, which makes it more pithy to implement the software components.
It consists of four parts:
-
Exchange component is one of the core components of the gateway project. It acts as a protocol converter between MQTT and PAN;
-
Data filter component provides some static filter, such as LinearFilter, EnumFilter etc. Once a filter is activated by user, each incoming/outgoing data frame will be filtered by it.
-
Plugin usually contains some user-defined business logic, such as sending a heartbeat, processing sensor data etc. Because every single data frame will pass to it, user can do anything they want according to the incoming data. Click here to get a depth understanding of the plugin developing.
-
PAN device Driver is a layer used for communication between Pan Device and Host CPU. Usually, the physical connection is a serial port. Now, it supports MeshBee v1.0.4 firmware and XBee.
Main features:
-
Can be ported to any platform that supports Python.
-
User-defined Qos, which ensure the reliability of data transmission.
-
Message forwarding is handled by Broker. User can focus on their application developing.
-
Pub/Sub model, one-to-many message deliver.
-
light-weight messaging protocol over TCP. It is designed for connections with remote locations where a “small code footprint” is required and/or network bandwidth is limited.
-
Support plugins expanding.
-
Support data filter.
-
Support any device that has a serial port.
-
Build-in Sqlite Database.
Getaway running flow
The following flow provides some basic procedures of how a gateway engine run.

Gateway configuration
Gateway program will read its configuration files at startup. We create a yaml file in root directory. Modify the following items to meet your request.
- yaml[‘pan’][‘port’]
Pan device serial port device ID in /dev.
- yaml[‘pan’][‘baudrate’’]
Baudrate of pan device serial port device.
- yaml[‘pan’][‘driver_class’]
Specified pan device driver
- yaml[‘mqtt’’][‘client_id’]
Gateway client ID
- yaml[‘mqtt’’][‘host’]
Broker Url
- yaml[‘mqtt’’][‘port’]
Broker TCP port number.