motor shield with multiple devices (SPI)

I’m trying to use the SPI interface to operate a motor shield along with a couple of OLEDs, and don’t know where to find the serial interface timing characteristics for the shield. The L298 datasheet seems to have only a couple of the numbers I need, and doesn’t include clock time, write time, address time, and chip select time, for instance. Does anyone have any ideas on where to find these? Thanks so much!

:open_mouth: Motor shield has occupied D10-D13, but those pins are not regarded as a SPI port. You can’t use Motor shield with other devices which need to use SPI port.

Jacket