Motor Shield affect all the pins

Hi, I am trying to get this
running along with this.

I have servo and sensor connected to groove shield, however motorshield somehow affect servo and sensor values!
According to the manual motorshield uses 5,4,6,7 pins, but it clearly does not.
Also this manual is very confusing and unclear.
I have these functions to run the motors:

[code]
void moveFwd()
{
digitalWrite(M1,HIGH);
digitalWrite(M2, HIGH);
analogWrite(E1, 200);
analogWrite(E2, 200);
delay(1000);
}

void moveLeft()
{
digitalWrite(M1,HIGH);
digitalWrite(M2, LOW);
analogWrite(E1, 200);
analogWrite(E2, 200);
delay(1000);
}

void moveRight()
{
digitalWrite(M1,LOW);
digitalWrite(M2, HIGH);
analogWrite(E1, 200);
analogWrite(E2, 200);
delay(1000);
}

void moveBwd()
{
digitalWrite(M1,LOW);
digitalWrite(M2, LOW);
analogWrite(E1, 200);
analogWrite(E2, 200);
delay(1000);
}

void halt()
{
analogWrite(E1, 0);
analogWrite(E2, 0);
}[/code]

Maybe I made some mistakes, as it not really working, because I cant understand speed control.

So I made different scetch for testing, witch just starting all the functions in a row with 10 seconds delay, but servo acting wierd, turning randomly. So here is my question - what is wrong with motorshield?

The motor shield uses pins 8,9,10,11,12,13 according to the wiki.

seeedstudio.com/wiki/Motor_Shield

It is wrong motorsield. I gave the link in the first post, its this shield - http://www.dfrobot.com/wiki/index.php?title=Arduino_Motor_Shield_(L298N)_(SKU:DRI0009)

Okay, first of all, you didn’t give the link in the first post.

Secondly, that’s the DFRobot motor shield. This is the Seeed Studio forum. You should probably ask them about it.