Has anyone successfully made the esp32se sense work with the Waveshare 2 inch LCD module or maybe any ST7789 display?? i posted some days ago about the problems I was having getting the XIAO esp32s3 working with the Waveshare 2 inch LCD Module;
Latest topics - Seeed Forum (seeedstudio.com)
I did finally get it working (kinda) but I still have a problem making it work correctly. I’m using Bodner’s tft_espi drivers from github. The LCD is 240x320 (defaulting to portrait). No matter what I do, all I can use of the screen is 240x240 pixels. I tried multiple combinations of 240x320, 320x240, and set_rotation. The set_rotation works in that it will change the format of the 240x240 box as verified from text printed to the screen. Theres a pic of the the setup to help with the explanation below. The setup does work well with the espc3 in the picture with the same sketch and drivers with just a single jumper connection changed so I know the LCD works.
My best guess is that there is just something strange going on with the s3/driver combination. In a lot of posts I see, the s3 is still not fully supported in a lot of areas and when it is, its usually the dev board that has pins that the XIAO s3 doesn’t have. (Not knocking the s3, just the way it is)