Opening onboard filesystem via FTP: filesystem seems to be bricked on brand new board W600-Pico?
=> main.py / boot.py /easyw600.py with 0 Bytes!
w600: soft reboot
__ __
\ \ /\ / /
\ \ / \ / /
\ \/ /\ \/ /
\ / \ /
/ /\ / /\
/ /\ \/ /\ \
/ / \ / \ \
/_/ \/ \_\
MicroPython v1.10-282-g6a9b3cb-dirty on 2019-09-17; WinnerMicro module with W600
Type “help()” for more information.
Seems to be an older version than:
MicroPython v1.10-284-g2eee4e2-dirty on 2019-11-08; WinnerMicro module with W600
Would try to reflash…
regards,
Juergen