I’m using the mmWave Human Detection Sensor Kit in a project for monitoring of elderly people. It works really well with the MR60BHA1 60GHz module, however, I would like to add fall detection as well, for which I could use the MR60FDA1 module.
Would it be feasible to combine these two modules on one board? The distance between the two modules would probably be less than 1 cm, and I fear this might influence the performance or accuracy of the mmWave radars on the two modules.