MISTAKE in Order Submission Guidelines

hello

i have found some contradiction between the order submission guidelines found in the table on fusion pcb page :

and the altium designer rules file

for example :
Minimum distance between pads and silkscreen is 0.178mm in the table ; while it is 0.254mm in the RUL file
Min Solder Mask Clearance is 0.13mm in the table ; while it is 0.254mm in the RUL file
Drilling Hole Diameter is 0.3 - 6.35 in the table ; while it is 0.025-2.54mm in RUL file
Minimum trace/vias/pads space is 0.1524 for 2 layer and 0.254mm for 4 layer ; while it is 0.2 in the RUL file
and many more

in addition some items are missing from the RUL and DRU files

please update them as soon as possible to help us deliver correct file from the first time

thanks