I bought one of the mini soldering irons, to use as a travel iron, and thought I’d post a couple thoughts about it.
First off, I do like it. It’s small, heats up quick quickly, and does a pretty good job.
The only problem that I have with it is that I want it (and it seems to be aimed) as a travel iron. Unfortunately, it’s not as easy to carry as one might like. You need an Allen wrench to insert a/o remove the tip, and you’ll definitely want to remove that tip before you pack it to avoid breaking the unit in half. Seeed is kind enough to provide the wrench and a spare screw, but no safe way to carry them. I’d suggest a pair of threaded holes to store the extra screws, and some way to insert the Allen wrench into the handle.
The bag that’s given with the unit is a nice touch, but it’s just a little too small to hold the handle, tips, power supply and power supply cord. That makes it rather useless. It only needs to be a little bit bigger…
Hello, I have a problem with my Mini Soldering iron. When powering it on, I press the button it wants me to press and then just resets itself, asking me to press the button again and so on. I thought it was a firmware glitch, entered DFU mode but dfu-util does not enumerate it and using it explicitly with vendor+device id yielded no results either. How to fix?
Thanks for sharing the review. I agree that for a tool marketed as a travel soldering iron, the portability details are just as important as the heating performance.
The Allen wrench storage is a great suggestion. Having to carry a separate tool and tiny screws increases the chances of losing them when working away from the bench. A slightly larger pouch would also make the kit much more practical.
I often use portable irons when assembling or modifying custom PCB prototypes from PCBWay, so a compact setup is definitely appealing. It sounds like the iron performs well overall, but a few small design changes could make it much more travel-friendly.