Trying 2 differents sdcard, one 8Go, one 64Go
Nothing is detected
The w10 driver is correctly installed, but no sd card detection
The ODYSSEY has a funky SD / SIM stacked card slot. Are you sure you are plugging the SD card into the SD card slot? I use the SIM slot, which is quite difficult to use, though reliable once the SIM card is inserted. There is a helpful guide printed on the board next to the slots.
Yes I’m sure of what I’ve done.
Btw the sdcard reader is unable to handle 64Go SDXC UHS Cards
That’s why.
Odyssey is limited to the olds 8Go
So maybe for a temporary backup only
Can you tell me the card model?